| Item |
Description |
| PR 1903366 |
Replace via API does not work as via User Interface |
| PR 1906499 |
No pattern in the 3D PDF (Test Case Specific) |
| PR 6758285 |
Add in groups and tabs remain after manually disconnecting an addin |
| PR 6764639 |
Implemented API GetRayIntersections for PartDocument |
| PR 1875930 |
API: wrong Text Box Width and Weight when adding multi line text |
| PR 1905243 |
Error in API Function SolidEdgeDraft::SectionsPtr->Count |
| PR 2201877 |
API: Parents Object of the fill pattern cannot be acquired |
| PR 6775244 |
Unpinned add-in docking pane can have incorrect text displayed |
| PR 1909277 |
ST5 license manager doesn't install on 2003 server |