Solid Edge Assembly Type Library
Angle Property
Description
Sets and returns the angular rotation of the referenced object.
Property type
Read-write property
Syntax
Visual Basic
Public Property Angle As Double
Remarks
For Rectangles, this value represents the rotation of the entire object. The angle is represented in Radians.
Example
Private Sub Form_Load()
    Dim objApp As SolidEdgeFramework.Application
    Dim objDoc As SolidEdgeAssembly.AssemblyDocument
    Dim objAngRel As SolidEdgeAssembly.AngularRelation3d
    Dim dblAngle As Double
    Const TESTFILE = "T:\vbtests\testcases\Sample.asm"
    ' Report errors
    Const PI = 3.14159265358979
    ' Create/get the application with specific settings
    On Error Resume Next
    Set objApp = GetObject(, "SolidEdge.Application")
    If Err Then
        Err.Clear
        Set objApp = CreateObject("SolidEdge.Application")
        Set objDoc = objApp.Documents.Add("SolidEdge.AssemblyDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    Call objDoc.Close
    ' opening an existing assembly document
    Set objDoc = objApp.Documents.Open(TESTFILE)
    ' getting the angular relation in the Relations3D collection object for the assembly document
    Set objAngRel = objDoc.Relations3d.Item(11)
    ' getting the angle defined in the angular relation and changing it
    dblAngle = objAngRel.Angle
    objAngRel.Angle = 3 * PI / 4
    ' USER DISPLAY
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objAngRel = Nothing
End Sub
See Also

AngularRelation3d Object  | AngularRelation3d Members

Send comments on this topic.