Solid Edge Assembly Type Library
GetNormal Method
Collapse All
Expand All
Solid Edge Assembly Type Library
>
AsmRefPlane Object
: GetNormal Method
Returns the array of unit-vectors that are normal to the reference plane.
Description
Returns unit ectors that are normal to the surface at a specified point.
Syntax
Visual Basic
Public Sub GetNormal( _ ByRef
Normal
() As Double _ )
Parameters
Normal
Returns the array of unit-vectors that are normal to the reference plane.
See Also
AsmRefPlane Object
|
AsmRefPlane Members
Send comments
on this topic.