| Solid Edge Assembly Type Library : AssemblyBody Object | 
|  GetFaceStyle2 | This method specifies whether user style preferences are returned for the referenced object. | 
|  GetReferenceKey | Returns a reference key for the referenced object. | 
|  Mirror | Mirror the referenced occurrence. | 
|  Application | Returns the active application object. | 
|  AssemblyBodyType | |
|  AttributeSets | Returns the AttributeSets collection object for the referenced object. | 
|  Body | Returns the Body object for the referenced object. | 
|  FaceStyle | Sets and returns the FaceStyle object for the referenced occurrence. | 
|  IsAttributeSetPresent | Returns True if a specified Attribute Set exists on the referenced object. | 
|  Name | Returns the name of the referenced object. | 
|  Parent | Returns the parent object for the referenced object. | 
|  Style | Returns the style for the referenced object. | 
|  TopLevelDocument | Returns the toplevel AssemblyDocument object. | 
|  Type | A member of the ObjectType constant set. | 
|  Visible | Controls the display of the referenced object. |