| Solid Edge Assembly Type Library : AssemblyFamilyMember Object |
AddOccurrence | Allows the referenced AssemblyFamilyMember object to use the MemberName of the Occurrence in its own definition. |
ExcludeObject | |
IncludeObject | |
RemoveExcludedAttachment | Removes the attachment from the referenced object. |
RemoveExcludedRelationship | Removes the relationship from the referenced object. |
SetMemberProperties | Sets member properties for the referenced object. |
SetVariableValue | Sets a variable to the specified value. |
Application | Returns the active application object. |
MemberName | Returns the member name of the referenced object. |
MemberProperties | Returns a specified property for the referenced object. |
Parent | Returns the parent object for the referenced object. |
Properties |