| Solid Edge Assembly Type Library : AssemblyFeaturesPattern Object | 
|  Delete | Deletes the referenced object. | 
|  GetParentFeatures | |
|  GetPatternType | |
|  GetProfile | |
|  Range | Returns the high and low range values for the referenced object. | 
|  RollToFeature | This method rolls the referenced object back to a specified feature. | 
|  SetParentFeatures | |
|  SetPatternType | |
|  SetProfile | 
|  Application | |
|  Edges | Returns a collection of edges of a specified type that belong to a model, a feature, or a topology collection of faces. The result of the Edges property is a topology collection. This topology collection is a temporary collection and is overwritten the next time the Edges, Faces, or FacesByRay property is used. | 
|  EdgesForScopePart | |
|  Faces | Returns a collection of faces of a specified type that belong to a model, a feature, or a topology object. The result of the Faces property is a topology collection. This topology collection is a temporary collection and is overwritten the next time the Edges, Faces, or FacesByRay property is used. | 
|  FacesByRay | Returns a collection of faces that are intersected by a specified vector. | 
|  FacesByRayForScopePart | |
|  FacesForScopePart | |
|  Name | Returns the name of the referenced object. | 
|  Parent | |
|  Suppress | Temporarily suppresses the referenced object. |