Solid Edge Assembly Type Library
FacesByRay Property
Description
Property type
Read-only property
Syntax
Visual Basic
Public Property FacesByRay( _
   ByVal Xorigin As Double, _
   ByVal Yorigin As Double, _
   ByVal Zorigin As Double, _
   ByVal Xdir As Double, _
   ByVal Ydir As Double, _
   ByVal Zdir As Double _
) As Object
Parameters
Xorigin
Yorigin
Zorigin
Xdir
Ydir
Zdir
See Also

AssemblyFeaturesRevolvedProtrusion Object  | AssemblyFeaturesRevolvedProtrusion Members

Send comments on this topic.