| Solid Edge Assembly Type Library : AssemblyThread Object |
Delete | Deletes the referenced object. |
GoTo | |
Range | Returns the high and low range values for the referenced object. |
Recompute | Recalculates the referenced object. |
Application | |
Edges | Returns a collection of edges of a specified type that belong to a model, a feature, or a topology collection of faces. The result of the Edges property is a topology collection. This topology collection is a temporary collection and is overwritten the next time the Edges, Faces, or FacesByRay property is used. |
Faces | Returns a collection of faces of a specified type that belong to a model, a feature, or a topology object. The result of the Faces property is a topology collection. This topology collection is a temporary collection and is overwritten the next time the Edges, Faces, or FacesByRay property is used. |
FacesByRay | Returns a collection of faces that are intersected by a specified vector. |
Holedata | |
Name | Returns the name of the referenced object. |
Parent | |
Suppress | Temporarily suppresses the referenced object. |
Visible | Specifies whether or not the referenced object is displayed to the screen. |