Solid Edge Assembly Type Library
FixedParallelOffset Property
Description
Specifies whether or not a fixed parallel offset is to be applied to the relationship.
Property type
Read-write property
Syntax
Visual Basic
Public Property FixedParallelOffset As Boolean
Remarks
If set to True, the constraint has fixed parallel offset. Otherwise, it has floating parallel offset.
See Also

AxialRelation3d Object  | AxialRelation3d Members

Send comments on this topic.