Solid Edge Assembly Type Library
Offset Property
Description
Sets or returns the distance that two parts are offset from one another.
Property type
Read-write property
Syntax
Visual Basic
Public Property Offset As Double
Remarks
If the parts are aligned, the Offset property can be either a positive or a negative value. If the parts are mated, the Offset property can only be a positive value.
See Also

AxialRelation3d Object  | AxialRelation3d Members

Send comments on this topic.