Solid Edge Assembly Type Library
ParallelOffset Property
Collapse All
Expand All
Solid Edge Assembly Type Library
>
AxialRelation3d Object
: ParallelOffset Property
Description
Specifies whether parallel offset is applied to the relationship.
Property type
Read-write property
Syntax
Visual Basic
Public Property ParallelOffset As Boolean
Remarks
If set to True, the constraint has parallel offset (and the FixedRotate property is ignored).
See Also
AxialRelation3d Object
|
AxialRelation3d Members
Send comments
on this topic.