Solid Edge Assembly Type Library
Select Method
If True, the current selection is replaced with a new selection that consists of the specified object. If False, the current selection is extended to include any previously selected objects and the specified object.
Description
Selects the referenced object in the active window.
Syntax
Visual Basic
Public Sub Select( _
   ByVal Replace As Boolean _
) 
Parameters
Replace
If True, the current selection is replaced with a new selection that consists of the specified object. If False, the current selection is extended to include any previously selected objects and the specified object.
Example
Private Sub Form_Load()
    Dim objApp As SolidEdgeFramework.Application
    Dim objDoc As SolidEdgeAssembly.AssemblyDocument
    Dim objAxialRel As SolidEdgeAssembly.AxialRelation3d
    Const TESTFILE = "T:\vbtests\testcases\Sample.asm"
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
        Set objDoc = objApp.Documents.Add("SolidEdge.AssemblyDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    Call objDoc.Close
    ' opening an existing assembly document
    Set objDoc = objApp.Documents.Open(TESTFILE)
    ' getting a particular axial relation in the collection
    Set objAxialRel = objDoc.Relations3d.Item(2)
    ' selecting the relation
    Call objAxialRel.Select(Replace:=True)
    ' USER DISPLAY
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objAxialRel = Nothing
End Sub
See Also

AxialRelation3d Object  | AxialRelation3d Members

Send comments on this topic.