| Solid Edge Assembly Type Library : Cable Object | 
|  CreatePhysicalConductor | |
|  Delete | Deletes the referenced object. | 
|  DeletePhysicalConductor | |
|  Edit | |
|  GetAdders | |
|  GetAllPaths | |
|  GetEndPoints | This method returns the start and end points of the referenced object. | 
|  GetOuterConductors | |
|  GetPaths | |
|  GetTopMostConductors | |
|  GetWires | |
|  Remove | |
|  SetAdders | 
|  Application | Returns the active application object. | 
|  AssemblyProperty | Returns the AssemblyProperty object used to store path attributes for the referenced object. | 
|  AttributeSets | Returns the AttributeSets collection object for the referenced object. | 
|  Color | This read-write property sets or returns the color in which the active object is drawn. The color is stored as a long integer and is created with the RGB function (red, green, and blue color intensities) or as an integer between 0 and 16 that represents standard colors. | 
|  CutLength | |
|  Description | |
|  Diameter | Sets and returns the diameter of the referenced object. | 
|  FromComponentName | |
|  FromTerminalName | |
|  Gage | |
|  IsAttributeSetPresent | Returns True if a specified Attribute Set exists on the referenced object. | 
|  LinearDensity | |
|  Mass | |
|  Material | Sets and returns the material. | 
|  MaterialType | |
|  MinimumBendRadius | |
|  Name | Returns the name of the referenced object. | 
|  NumberOfConductors | |
|  OuterDiameter | Sets and returns the outer diameter of the referenced object. | 
|  Parent | Returns the parent object for the referenced object. | 
|  PartNumber | |
|  ToComponentName | |
|  ToTerminalName | |
|  TrueLength | |
|  Type | Specifies the type of the object being referenced. | 
|  UseGlobalAdders | |
|  Visible | Specifies whether or not the referenced object is displayed to the screen. |