| Solid Edge Assembly Type Library : CurveSegment Object | 
|  AddPathSegment | Adds a path segment. | 
|  Delete | Deletes the referenced object. | 
|  GetPathSegment | Returns the input object specified by the index. | 
|  HidePathSegments | Hides the input path segments. | 
|  RemovePathSegment | Removes a path segment. | 
|  ShowPathSegments | Shows the input path segments. | 
|  Application | Returns the active application object. | 
|  AttributeSets | Returns the AttributeSets collection object for the referenced object. | 
|  EndDerivativeMagnitude | Sets and returns the end derivative magnitude. | 
|  IsAttributeSetPresent | Returns True if a specified Attribute Set exists on the referenced object. | 
|  Parent | Returns the parent object for the referenced object. | 
|  PathSegmentsCount | Returns the number of input path objects. | 
|  StartDerivativeMagnitude | Sets and returns the start derivative magnitude. | 
|  Type | Specifies the type of the object being referenced. | 
|  Validation | Determines curve validity. | 
|  WhichKeypoints | Specifies the keypoints used to compute the curve. |