| Solid Edge Assembly Type Library : GearRelation3d Object | 
|  Delete | Deletes the referenced object. | 
|  Flip | |
|  GetElement1 | Returns the first element in this relationship. | 
|  GetElement2 | Returns the second element in this relationship. | 
|  GetGeometry1 | Returns the geometry of the referenced object. | 
|  GetGeometry2 | Returns the geometry of the referenced object. | 
|  Select | Selects the referenced object in the active window. | 
|  Application | Returns the active application object. | 
|  AttributeSets | Returns the AttributeSets collection object for the referenced object. | 
|  DetailedStatus | Returns the detailed status of the Relation3d object. | 
|  Index | Returns the numeric index for the active object. | 
|  IsAttributeSetPresent | Returns True if a specified Attribute Set exists on the referenced object. | 
|  Occurrence1 | Returns the first Occurrence object for the referenced relationship object. | 
|  Occurrence2 | Returns the second Occurrence object for the referenced relationship object. | 
|  Parent | Returns the parent object for the referenced object. | 
|  RatioValue1 | This property sets the first gear ratio value. | 
|  RatioValue2 | This property sets the second gear ratio value. | 
|  Status | Returns the status of the specified object. | 
|  Suppress | Temporarily suppresses the referenced object. | 
|  Type | Specifies the type of the object being referenced. |