Solid Edge Assembly Type Library
GetAdjustablePart Method
Description
Returns the adjustable part object.
Syntax
Visual Basic
Public Function GetAdjustablePart() As AdjustablePart
Example
Imports System.IO
Imports System.Runtime.InteropServices

Module Example
    <STAThread()> _
    Sub Main()
        Dim objApplication As SolidEdgeFramework.Application = Nothing
        Dim objDocuments As SolidEdgeFramework.Documents = Nothing
        Dim objAssemblyDocument As SolidEdgeAssembly.AssemblyDocument = Nothing
        Dim objOccurrences As SolidEdgeAssembly.Occurrences = Nothing
        Dim objOccurrence As SolidEdgeAssembly.Occurrence = Nothing
        Dim objAdjustablePart As SolidEdgeAssembly.AdjustablePart = Nothing
        Dim bAdjustToFit As Boolean

        Try
            OleMessageFilter.Register()

            ' Start Solid Edge
            objApplication = Activator.CreateInstance(Type.GetTypeFromProgID("SolidEdge.Application"))
            objApplication.Visible = True
            objDocuments = objApplication.Documents

            objAssemblyDocument = objDocuments.Open("anyfilename.asm")
            objOccurrences = objAssemblyDocument.Occurrences
            objOccurrence = objOccurrences.Item(1)
            objAdjustablePart = objOccurrence.GetAdjustablePart()
            bAdjustToFit = objAdjustablePart.AdjustToFit
            ' Demo toggling the AdjustToFit property.
            objAdjustablePart.AdjustToFit = Not bAdjustToFit
        Catch ex As Exception
            Console.WriteLine(ex.Message)
        Finally
            OleMessageFilter.Revoke()
        End Try
    End Sub
End Module
See Also

Occurrence Object  | Occurrence Members

Send comments on this topic.