Solid Edge Assembly Type Library
IsNongraphic Property
Description
Returns True if the referenced Occurrence is non-graphic, false if it is not.
Property type
Read-only property
Syntax
Visual Basic
Public Property IsNongraphic As Boolean
Remarks
Returns True if the Occurrence is non-graphic, false if it is not.
See Also

Occurrence Object  | Occurrence Members

Send comments on this topic.