Solid Edge Assembly Type Library
Select Method
If True, the current selection is replaced with a new selection that consists of the specified object. If False, the current selection is extended to include any previously selected objects and the specified object.
Description
Selects the referenced object in the active window.
Syntax
Visual Basic
Public Sub Select( _
   ByVal Replace As Boolean _
) 
Parameters
Replace
If True, the current selection is replaced with a new selection that consists of the specified object. If False, the current selection is extended to include any previously selected objects and the specified object.
Example
Private Sub Form_Load()
    Dim objApp As SolidEdgeFramework.Application
    Dim objDoc As SolidEdgeAssembly.AssemblyDocument
    Dim objPart As SolidEdgeAssembly.Occurrence
    Const TESTFILE = "T:\vbtests\testcases\Sample.asm"
    ' Report errors
    Const PI = 3.14159265358979
    ' Create/get the application with specific settings
    On Error Resume Next
    Set objApp = GetObject(, "SolidEdge.Application")
    If Err Then
        Err.Clear
        Set objApp = CreateObject("SolidEdge.Application")
        Set objDoc = objApp.Documents.Add("SolidEdge.AssemblyDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    Call objDoc.Close
    ' opening an existing assembly file
    Set objDoc = objApp.Documents.Open(TESTFILE)
    ' getting a part in the assembly
    Set objPart = objDoc.Occurrences.Item(3)
    ' selecting the placed part in the assembly
    Call objPart.Select(Replace:=False)
    ' USER DISPLAY
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objPart = Nothing
End Sub
See Also

Occurrence Object  | Occurrence Members

Send comments on this topic.