|  Application | Returns the active application object. | 
|  AttributeSets | Returns the AttributeSets collection object for the referenced object. | 
|  DisplayInDrawings | Controls whether or not the referenced part or assembly is visible in the draft environment. | 
|  DisplayInSubAssembly | Specifies whether the referenced Part is shown or hidden when this assembly is inserted into another assembly. | 
|  FaceStyle | Sets and returns the FaceStyle object for the referenced Occurrence. | 
|  IncludeInBom | Controls whether or not the referenced part is included in reports. | 
|  IncludeInPhysicalProperties | Controls whether or not the referenced Part is included in physical property calculations. | 
|  Index | Returns the numeric index for the active object. | 
|  IsAttributeSetPresent | Returns True if a specified Attribute Set exists on the referenced object. | 
|  IsForeign | Specifies whether or not the referenced Part orginated from an application other than Solid Edge. | 
|  Locatable | Sets and returns the referenced object's locatable state. | 
|  Name | Returns the name of the referenced object. | 
|  Parent | Returns the parent object for the referenced object. | 
|  PartDocument | Returns the PartDocument object for the active Part. | 
|  PartFileName | Returns the name of the data file for the PartDocument object of the active part. | 
|  Quantity | Returns the number of occurrences of the referenced object. | 
|  ReferenceOnly | Returns the 'reference-only' state of the active Part. | 
|  Relations3d | Returns a collection of Relations3d objects for the referenced Part. | 
|  Status | Returns the status (a member of the PartStatusConstants constant set) of the referenced Part. | 
|  Style | Returns the style for the referenced object. | 
|  Subassembly | Returns True if the referenced object is a subassembly. | 
|  Type | A member of the ObjectType constant set. | 
|  Visible | Controls the display of the referenced object. |