Solid Edge Assembly Type Library
StartpointMagnitude Property
Description
Sets and returns the direction and degree of influence of the StartpointEdge on the curvature of the curve at the startpoint.
Property type
Read-only property
Syntax
Visual Basic
Public Property StartpointMagnitude As Double
Remarks
This value is meaningful only if the StartpointEndCondition is seKeypointEndConditionTangent.
See Also

Path Object  | Path Members  | Solid Edge V18 - What's New

Send comments on this topic.