|  Application | Returns the active application object. | 
|  AttributeSets | Returns the AttributeSets collection object for the referenced object. | 
|  DetailedStatus | Returns the detailed status of the Relation3d object. | 
|  Index | Returns the numeric index for the active object. | 
|  IsAttributeSetPresent | Returns True if a specified Attribute Set exists on the referenced object. | 
|  Occurrence1 | Returns the first Occurrence object for the referenced relationship object. | 
|  Occurrence2 | Returns the second Occurrence object for the referenced relationship object. | 
|  Parent | Returns the parent object for the referenced object. | 
|  RangedOffset |  | 
|  RangeHigh |  | 
|  RangeLow |  | 
|  Status | Returns the status (a member of the Relation3dStatusConstants constant set) of the referenced Part. | 
|  Suppress | Temporarily suppresses the referenced object. | 
|  Type | A member of the ObjectType constant set. |