| Solid Edge Assembly Type Library : SegmentDirectionRelation3d Object | 
|  Delete | Deletes the referenced object. | 
|  GetElement1 | Returns the first of the two elements constrained by the referenced SegmentDirectionRelation3d object. | 
|  GetElement2 | Returns the second of the two elements constrained by the referenced SegmentDirectionRelation3d object. | 
|  Select | Selects the referenced object in the active window. | 
|  Application | Returns the active application object. | 
|  AttributeSets | Returns the AttributeSets collection object for the referenced object. | 
|  DirectionType | Returns the direction type (parallel, perpendicular, or coincident) for the referenced SegmentDirectionRelation3d object. | 
|  Index | Returns the numeric index for the active object. | 
|  IsAttributeSetPresent | Returns True if a specified Attribute Set exists on the referenced object. | 
|  Parent | Returns the parent object for the referenced object. | 
|  Status | Returns the status of the specified object. | 
|  Type | Specifies the type of the object being referenced. |