| Solid Edge Assembly Type Library : SegmentRadiusRelation3d Object | 
|  Delete | Deletes the referenced object. | 
|  GetElement1 | |
|  Select | Selects the referenced object in the active window. | 
|  Application | Returns the active application object. | 
|  ArcSegment | Returns the ArcSegment object for the referenced SegmentRadiusRelation3d object. | 
|  AttributeSets | Returns the AttributeSets collection object for the referenced object. | 
|  Dimension | |
|  Index | Returns the numeric index for the active object. | 
|  IsAttributeSetPresent | Returns True if a specified Attribute Set exists on the referenced object. | 
|  Parent | Returns the parent object for the referenced object. | 
|  Radius | Returns the radius of the referenced object. | 
|  Status | Returns the status of the specified object. | 
|  Type | Specifies the type of the object being referenced. |