| Solid Edge Assembly Type Library : SegmentTangentRelation3d Object |
Delete | Deletes the referenced object. |
GetElement1 | Returns the first of the two elements constrained by the referenced SegmentDirectionRelation3d object. |
GetElement2 | Returns the second of the two elements constrained by the referenced SegmentDirectionRelation3d object. |
Select | Selects the referenced object in the active window. |
Application | Returns the active application object. |
AttributeSets | Returns the AttributeSets collection object for the referenced object. |
Index | Returns the numeric index for the active object. |
IsAttributeSetPresent | Returns True if a specified Attribute Set exists on the referenced object. |
Parent | Returns the parent object for the referenced object. |
Status | Returns the status of the specified object. |
Type | Specifies the type of the object being referenced. |