Solid Edge Assembly Type Library
DisplayCenterline Property
Description
Property type
Read-write property
Syntax
Visual Basic
Public Property DisplayCenterline As Boolean
Example
Imports System.IO
Imports System.Runtime.InteropServices

Module Example
    <STAThread()> _
    Sub Main()

        Dim objApplication As SolidEdgeFramework.Application = Nothing
        Dim objAssemblyDocument As SolidEdgeAssembly.AssemblyDocument = Nothing
        Dim objOccurrences As SolidEdgeAssembly.Occurrences = Nothing
        Dim objOccurrence As SolidEdgeAssembly.Occurrence = Nothing
        Dim objSubOccurrences As SolidEdgeAssembly.SubOccurrences = Nothing
        Dim objSubOccurrence As SolidEdgeAssembly.SubOccurrence = Nothing

        Try
            OleMessageFilter.Register()

            objApplication = Marshal.GetActiveObject("SolidEdge.Application")
            objAssemblyDocument = objApplication.ActiveDocument
            objOccurrences = objAssemblyDocument.Occurrences

            For Each objOccurrence In objOccurrences
                If (objOccurrence.DisplayCenterline = True) Then
                    objOccurrence.DisplayCenterline = False
                Else
                    objOccurrence.DisplayCenterline = True
                End If
                If Not (objOccurrence.SubOccurrences Is Nothing) Then
                    objSubOccurrences = objOccurrence.SubOccurrences
                    For Each objSubOccurrence In objSubOccurrences
                        If (objSubOccurrence.DisplayCenterline = True) Then
                            objSubOccurrence.DisplayCenterline = False
                        Else
                            objSubOccurrence.DisplayCenterline = True
                        End If
                    Next
                End If
            Next

        Catch ex As Exception
            Console.WriteLine(ex.Message)
        Finally
            OleMessageFilter.Revoke()
        End Try
    End Sub
End Module
See Also

SubOccurrence Object  | SubOccurrence Members  | Solid Edge ST5 - What's New

Send comments on this topic.