Solid Edge Assembly Type Library
GetMatrix Method
Collapse All
Expand All
Solid Edge Assembly Type Library
>
SubOccurrence Object
: GetMatrix Method
Returns the 4x4 array that specifies the position and orientation of the part. This is a single-dimension Double array that contains 16 elements.
Description
Returns the transformation matrix for the referenced suboccurrence.
Syntax
Visual Basic
Public Sub GetMatrix( _ ByRef
Matrix
() As Double _ )
Parameters
Matrix
Returns the 4x4 array that specifies the position and orientation of the part. This is a single-dimension Double array that contains 16 elements.
Remarks
The matrix defines the current position and orientation of the object.
See Also
SubOccurrence Object
|
SubOccurrence Members
Send comments
on this topic.