| Solid Edge Assembly Type Library > SubOccurrence Object : HasBodyOverride Property |
| Visual Basic |
|---|
Public Property HasBodyOverride As Boolean |
When objXYZ.HasBodyOverride=True, the override body may be accessed by the method objXYZ.Body where objXYZ is an object of type SubOccurrence and objXYZ.Subassembly=FALSE.
This method returns the body in the assembly space where the override was created and not in the original part space, therefore SubOccurrence transform should not be directly applied to the body geometry.
Member of SolidEdgeAssembly.SubOccurrence
Property HasBodyOverride As Boolean (read-only)