Solid Edge Assembly Type Library
Range Method
Description
Syntax
Visual Basic
Public Sub Range( _
   ByRef x_min As Double, _
   ByRef y_min As Double, _
   ByRef z_min As Double, _
   ByRef x_max As Double, _
   ByRef y_max As Double, _
   ByRef z_max As Double _
) 
Parameters
x_min
y_min
z_min
x_max
y_max
z_max
See Also

SubOccurrence Object  | SubOccurrence Members  | Solid Edge ST5 - What's New

Send comments on this topic.