| Solid Edge Assembly Type Library : VirtualComponentOccurrence Object |
Delete | Delete this Virtual Component occurrence. |
GetOrigin | |
GetOriginByKeypoints | |
GetViewDefinition | |
Hide | Hides the component selected. |
HideAll | Hides the component selected and any components under it. |
IsMaster | |
IsVisible | This method returns True if the referenced object is visible and False if not. |
MoveTo | Move this Virtual Component occurrence to a different Virtual Component. |
PositionComponent | |
ReplaceComponent | |
SetOrigin | |
SetOriginByKeypoints | |
SetViewDefinition | |
Show | Shows the component selected. |
ShowAll | Shows the component selected and any components under it. |
Angle | The angular rotation of the referenced object. |
Application | |
AttributeSets | Returns the AttributeSets collection object for the referenced object. |
IsAttributeSetPresent | Returns True if a specified Attribute Set exists on the referenced object. |
IsPositioned | |
IsPreDefined | |
Name | Retrieve the name of the virtual component for which this is a Virtual Component occurrence. |
Parent | |
Type | Specifies the type of the object being referenced. |
VirtualComponent | Retrieve the virtual component for which this is a Virtual Component occurrence. |