| Solid Edge Assembly Type Library : VirtualComponent Object |
Delete | Delete this Virtual Component and all its Virtual Component occurrences. |
GetGeometry | |
RemoveGeometry | |
SetGeometry | |
UpdateComponent |
Application | |
AttributeSets | Returns the AttributeSets collection object for the referenced object. |
IsAttributeSetPresent | Returns True if a specified Attribute Set exists on the referenced object. |
Name | Specify or retrieve the name of the Virtual Component. |
Parent | |
Properties | Retrieve the collection of properties for this Virtual Component. |
PublishPath | Specify or retrieve the path to the directory in which to create the document file when the Virtual Component is published. |
TemplateName | Specify or retrieve the template file name to use to create the document file when the Virtual Component is published. |
Type | Specifies the type of the object being referenced. |
VirtualComponentOccurrences | Retrieve the collection of Virtual Component occurrences for this Virtual Component. |
VirtualComponentType | Retrieve the Virtual Component type which may be seVirtualComponentType_Assembly, seVirtualComponentTypeType_Part, or seVirtualComponentType_Sheetmetal. |