|  Application | Returns the active application object. | 
|  AssemblyProperty | Returns the AssemblyProperty object. | 
|  CableMaster | Returns the cable master WirePath object. | 
|  CableMembers | Returns the WirePathCableMembers collection object. | 
|  Color | Sets and returns the color in which the active object is drawn. | 
|  ColorName | Sets and returns the color name. | 
|  Diameter | Sets and returns the diameter. | 
|  EndConnector | Sets and returns the end connector string. | 
|  Length | Specifies the length of the referenced object. | 
|  Material | Sets and returns the material. | 
|  Name | Returns the name of the referenced object. | 
|  Parent | Returns the parent object for the referenced object. | 
|  Segments | Returns the WirePathSegments collection object. | 
|  StartConnector | Sets and returns the start connector string. | 
|  Type | Sets and returns the wire path type. | 
|  Visible | Specifies whether or not the referenced object is displayed to the screen. |