|  Application |  | 
|  Caption |  | 
|  CaptionDefinitionText | Sets and returns the definition text for the caption. Definition text can contain codes for Property Text and Symbols. | 
|  CaptionDisplayedText | Returns the text for the caption as displayed after processing Property Text and Symbols. | 
|  DisplayCaption | Specifies whether or not the caption of the referenced object is displayed. | 
|  DisplayType | Specifies the display type for the CuttingPlane. | 
|  DisplayViewSheetNumber | Sets and returns whether the ViewSheetNumber definition string is displayed in the caption. | 
|  FoldSegment | Specifies the 1-based index of the segment that defines the fold direction of the view. | 
|  Layer | Sets and returns the named layer on which the referenced object resides. | 
|  LineDisplayStyle | Sets and returns the display style for the cutting plane. | 
|  LineType | Sets and returns the line display type of the drawing view. | 
|  LineWidth | Sets and returns the line width (in paper space units) for the referenced object. | 
|  Profile | Returns the profile associated with the parent object. | 
|  SectionView | Returns the section view associated with the cutting plane line. | 
|  SourceDrawingView | Returns the DrawingView object from which the detail drawing view is derived. | 
|  StyleName | Sets and returns the name of the style that is applied to the referenced object. | 
|  TerminatorRatio | Sets and returns the terminator ratio for the active ViewPlane object. | 
|  TerminatorType | Sets and returns the type of terminator for both origin and measure for the referenced DimensionStyle object. | 
|  TextColor | Sets and returns the color of the text for the caption of the referenced object. | 
|  TextFont | Sets and returns the text font of the caption of the referenced object. | 
|  TextFontStyle | Sets and returns the text font style of the caption of the referenced object. | 
|  TextHeight | Sets and returns the text height of the caption of the referenced object. | 
|  TextRatio | Sets and returns the text ratio of the caption of the referenced object. | 
|  ThickLineArrowOffset | Sets and returns offset distance (0.0 - 1.0) for the arrow terminator. | 
|  ThickLineLengthRatio | Sets and returns multiplication factor for the line length. Ex. line length = ThickLineLengthRatio x font size. | 
|  ViewSheetNumberDefinitionText | Sets and returns the View Sheet Number (%VN) definition string.  This is intended for use with %{View Sheet Number|DV} property text and may include other formatting options. | 
|  ViewSheetNumberLocation | Sets and returns the Sheet Number Location of the cutting plane. | 
|  ViewSide | Sets or returns the side of the free end of the fold segment that determines the direction of the view. This will use the existing enumerated type SectionViewProfileSide, with only igLeftProfileSide and igRightProfileSide being valid. If the view has not been created it will have a default value of igLeftProfileSide. |