|  Application | Returns the active application object. | 
|  AttributeSets | Returns the AttributeSets collection object for the referenced object. | 
|  BendAngle | Returns the bend angle from the underlying sheet metal model. | 
|  BendRadius | Returns the bend radius from the underlying sheet metal model. | 
|  Document | Returns the document to which the referenced object belongs. | 
|  DrawingView | Returns the DrawingView for this object. | 
|  EdgeType | Returns the EdgeType for this object. | 
|  IsAttributeSetPresent | Returns True if a specified Attribute Set exists on the referenced object. | 
|  Key | Returns a key (a string) to find the object relative to its owning parents. | 
|  KeyPointCount | Returns the number of keypoints/handles that are supported by the referenced object. | 
|  ModelMember | Returns the ModelMember for this object. | 
|  ModelWelds | Returns the ModelWelds collection object. | 
|  Name | Returns the name of the referenced object. | 
|  Orientation | Sets and returns the direction in which an arc or elliptical arc is drawn. | 
|  Radius | Returns the radius of the referenced object. | 
|  Reference | Returns a Reference object for this object. | 
|  Relationships | Returns a collection of objects that are related to the referenced graphic object. | 
|  SegmentedStyleCount | Returns the number of segmented styles defined for the referenced graphic object. | 
|  StartAngle | Sets and returns the angle, in radians, at which the arc begins along a circle or ellipse with regard to the major axis. | 
|  SweepAngle | Sets and returns the angle, in radians, at which the arc ends along a circle or ellipse with regard to the major axis of the referenced object. | 
|  Type | Specifies the type of the object being referenced. |