Application | Returns the active application object. |
Area | Returns the area of the referenced object. |
AttributeSets | Returns the AttributeSets collection object for the referenced object. |
BendAngle | Returns the bend angle from the underlying sheet metal model. |
BendRadius | Returns the bend radius from the underlying sheet metal model. |
Circumference | Returns the dimension along the line of a circle or ellipse. |
Document | Returns the document to which the referenced object belongs. |
DrawingView | Returns the DrawingView for this object. |
EdgeType | Returns the EdgeType for this object. |
IsAttributeSetPresent | Returns True if a specified Attribute Set exists on the referenced object. |
Key | Returns a key (a string) to find the object relative to its owning parents. |
KeyPointCount | Returns the number of keypoints/handles that are supported by the referenced object. |
MajorRadius | Sets and returns the radius of the major axis for the referenced object. |
MinorMajorRatio | Sets and returns the ratio of the minor axis length relative to the length of the major axis for the referenced object. |
MinorRadius | Sets and returns the radius of the minor axis for the referenced object. |
ModelMember | Returns the ModelMember for this object. |
ModelWelds | Returns the ModelWelds collection object. |
Name | Returns the name of the referenced object. |
Orientation | Sets and returns the direction in which an arc or elliptical arc is drawn. |
Reference | Returns a Reference object for this object. |
Relationships | Returns a collection of objects that are related to the referenced graphic object. |
RotationAngle | Sets and returns the angle, in radians, at which the object is rotated along its major axis. |
SegmentedStyleCount | Returns the number of segmented styles defined for the referenced graphic object. |
Type | Specifies the type of the object being referenced. |