Solid Edge Draft Type Library
Circumference Property
Collapse All
Expand All
Solid Edge Draft Type Library
>
DVEllipse2d Object
: Circumference Property
Description
Returns the dimension along the line of a circle or ellipse.
Property type
Read-only property
Syntax
Visual Basic
Public Property Circumference As Double
Remarks
The circumference value is always around the complete object for objects that are partially trimmed or hidden.
See Also
DVEllipse2d Object
|
DVEllipse2d Members
Send comments
on this topic.