Private Sub btnImportStyles_Click(sender As System.Object, e As System.EventArgs) Handles btnImportStyles.Click
    Dim objApplication As SolidEdgeFramework.Application = Nothing
    Dim objDraftDoc As SolidEdgeDraft.DraftDocument = Nothing
    Dim objDoc2 As SolidEdgeDraft.DraftDocument
    Dim objType As Type = Nothing
    Try
        objApplication = GetObject(, "SolidEdge.Application")
        If objApplication Is Nothing Then
            ' Get the type from the Solid Edge ProgID
            objType = Type.GetTypeFromProgID("SolidEdge.Application")
            ' Start Solid Edge
            objApplication = Activator.CreateInstance(objType)
            ' Make Solid Edge visible
            objApplication.Visible = True
        End If
        objDraftDoc = objApplication.ActiveDocument
        objDoc2 = objApplication.Documents.Open("C:\Program Files (x86)\Solid Edge ST6\Training\stddb3d.dft")
        Call objDraftDoc.ImportStyles2(SolidEdgeFramework.seStyleTypeConstants.igDimensionStyle, False, objDoc2)
        Call objDraftDoc.ImportStyles2(SolidEdgeFramework.seStyleTypeConstants.igLineStyle, False, objDoc2)
        Call objDraftDoc.ImportStyles2(SolidEdgeFramework.seStyleTypeConstants.igTableStyle, True, objDoc2)
        Call objDraftDoc.ImportStyles2(SolidEdgeFramework.seStyleTypeConstants.igFillStyle, True, objDoc2)
        Call objDraftDoc.ImportStyles2(SolidEdgeFramework.seStyleTypeConstants.igHatchStyle, True, objDoc2)
        Call objDraftDoc.ImportStyles2(SolidEdgeFramework.seStyleTypeConstants.igDrawingViewStyle, True, objDoc2)
        Call objDraftDoc.ImportStyles2(SolidEdgeFramework.seStyleTypeConstants.igTextStyle, True, objDoc2)
    Catch ex As Exception
        MsgBox(ex.ToString)
    End Try
End Sub