ActivePrintingSheet | Returns the Sheet object currently being printed. |
ActiveSection | Returns the active sheet's Section object. Sheets are grouped into sections: WorkingSection, BackgroundSection, and 2dModelSection. |
ActiveSectionType | Specifies the type of Section that the active sheet is a member of. |
ActiveSheet | Returns the active Sheet object. |
ActiveSketch | Returns the active Sketch object. |
AddInsStorage | Returns an IUnknown pointer to the object that implements the IStorage corresponding to the add-in substorage for the referenced object. |
Application | Returns the active application object. |
AttributeQuery | Returns the AttributeQuery object. |
Blocks | Returns the collection of blocks in the document. |
BlockTableEvents | Contains the AfterUpdate event. |
BlockTables | Returns the associated BlockTables object for the referenced DraftDocument object. |
ConnectorTableEvents | Contains the AfterUpdate event. |
ConnectorTables | Returns the associated ConnectorTables object for the referenced DraftDocument object. |
CreatedVersion | Returns the version of Solid Edge that was used to create the referenced document. |
DashStyles | This read-only property returns the DashStyles collection object for the referenced DraftDocument object. |
DimensionStyles | Returns the DimensionStyles collection object for the referenced document. |
Dirty | Specifies whether or not the referenced document has been modified since the last time it was saved. |
DisplayAlignmentIndicator | Sets and returns whether or not the alignment indicator is displayed. |
DisplayRelationshipHandles | Sets and returns whether or not relationship handles are displayed. |
DocumentEvents | Returns the DocumentEvents object for the referenced document object. |
DraftBendTableEvents | Contains the AfterUpdate event. |
DraftBendTables | Returns the associated DraftBendTables object for the referenced DraftDocument object. |
DrawingViewEvents | Returns the DrawingViewEvents object for the referenced DraftDocument object. |
DrawingViewStyles | Returns the DrawingViewStyles collection object for the referenced document. |
FeatureControlFrameDataSets | Returns the FeatureControlFrameDataSets collection object for the referenced document. |
FilePreferences | Get and set file level preferences. |
FillStyles | Returns the FillStyles collection object for the referenced document. |
FullName | Returns the name and path of the referenced object. |
HatchPatternStyles | Returns the HatchPatternStyles collection object for the referenced document. |
HighlightSets | Returns the HighlightSets collection object for the referenced document object. |
HoleTables | Returns the HoleTables collection object. |
InactiveDrawingViewMode | Sets and returns the inactive drawing view mode on the document. |
InPlaceActivated | Specifies whether or not the referenced document is in-place activated. |
IsTemplate | Specifies whether or not the referenced document is a template. |
LastSavedVersion | Returns the version of Solid Edge that was used the last time the referenced document was saved. |
LinearStyles | Returns the LinearStyles collection object for the referenced document. |
MaintainRelationships | Returns whether maintain relationships is enabled or disabled |
ModelLinks | Returns the ModelLinks collection object for the referenced document. |
Name | Returns the name of the referenced object. |
Parent | Returns the parent object for the referenced object. |
PartsListEvents | Contains the AfterUpdate event. |
PartsLists | Returns the associated PartsLists object for the referenced DraftDocument object. |
Path | Returns the directory path name of the referenced document. |
Properties | For document objects, returns the PropertiesCollection colletion object. For Variables, sets and returns the variable properties. |
QuicksheetTemplateCount | Returns the count of Quicksheet drawing views. |
ReadOnly | Specifies whether or not the referenced document has been opened as read-only. |
RootStorage | Returns the IUnknown pointer to the object implementing the root storage of the referenced document. |
RoutingSlip | Returns the RoutingSlip object for the referenced document. |
Sections | Returns the Sections collection object for the referenced document. Sheets are grouped into sections: WorkingSection, BackgroundSection, and 2dModelSection. |
SelectSet | Returns the current selection set for the referenced document. |
SheetGroups | Returns a collection of working sheet groups. |
Sheets | Returns a collection of sheets that belong to the referenced object. |
SmartFrame2dStyles | Returns the SmartFrames2d collection object for the referenced document. |
Status | Returns the status of the specified object. |
SummaryInfo | Returns a SheetSummaryInfo object to provide access to descriptive properties for the referenced document. |
SurfaceFinishSymbolDataSets | Returns the SurfaceFinishSymbolDataSets collection object for the referenced document. |
SymbolProperties | Returns the SymbolProperties collection object for the referenced document. |
Tables | Returns the collection of user tables in the document. |
TextCharStyles | Returns the TextCharStyles collection object for the referenced document. |
TextStyles | Returns the TextStyles collection object for the referenced document. |
Type | Specifies the type of the object being referenced. |
UndoSteps | This read-write Long property sets and returns the number of undo steps for the referenced document object. |
UnitsOfMeasure | Returns the UnitsOfMeasure object for the referenced document. |
Variables | Returns the Variables collection object for the referenced document. |
WeldSymbolDataSets | Returns the WeldSymbolDataSets collection object for the referenced document. |
Windows | Returns the Windows collection object. |