Private Sub btnSymbolFileOrigin_Click(sender As System.Object, e As System.EventArgs) Handles btnSymbolFileOrigin.Click
Dim objApplication As SolidEdgeFramework.Application = Nothing
Dim objDraftDoc As SolidEdgeDraft.DraftDocument = Nothing
Dim xOrigin As Double
Dim yOrigin As Double
Dim objType As Type = Nothing
Try
'Connect to a running instance of Solid Edge
objApplication = Marshal.GetActiveObject("SolidEdge.Application")
If objApplication Is Nothing Then
' Get the type from the Solid Edge ProgID
objType = Type.GetTypeFromProgID("SolidEdge.Application")
' Start Solid Edge
objApplication = Activator.CreateInstance(objType)
' Make Solid Edge visible
objApplication.Visible = True
End If
'Get a reference to active draft document
objDraftDoc = objApplication.ActiveDocument
Call objDraftDoc.SetSymbolFileOrigin(0.12, 0.15)
Call objDraftDoc.GetSymbolFileOrigin(xOrigin, yOrigin)
Catch ex As Exception
MsgBox(ex.ToString)
End Try
End Sub