Solid Edge Draft Type Library
Item Method
Variant (input) index.
Description
The items in a collection.
Syntax
Visual Basic
Public Function Item( _
   ByVal Index As Variant _
) As DrawingView
Parameters
Index
Variant (input) index.
Example
Imports System.IO
Imports System.Runtime.InteropServices

Module Example
    <STAThread()> _
    Sub Main()
        Dim objApplication As SolidEdgeFramework.Application = Nothing
        Dim objDraftDocument As SolidEdgeDraft.DraftDocument
        Dim objSheet As SolidEdgeDraft.Sheet = Nothing
        Dim objDrawingViews As SolidEdgeDraft.DrawingViews = Nothing
        Dim objDrawingView As SolidEdgeDraft.DrawingView = Nothing

        Try
            OleMessageFilter.Register()

            objApplication = Marshal.GetActiveObject("SolidEdge.Application")
            objDraftDocument = objApplication.ActiveDocument
            objSheet = objDraftDocument.ActiveSheet
            objDrawingViews = objSheet.DrawingViews
            objDrawingView = objDrawingViews.Item(1)

        Catch ex As Exception
            Console.WriteLine(ex.Message)
        Finally
            OleMessageFilter.Revoke()
        End Try
    End Sub
End Module
See Also

DrawingViews Collection  | DrawingViews Members

Send comments on this topic.