|  Add2dModelView | This method creates a 2D Model view as a DrawingView object. | 
|  AddAssemblyView | Adds an assembly drawing view based on the ViewType and an optional configuration name. | 
|  AddByAuxiliaryFold | Creates an auxiliary DrawingView object and a ViewPlane object from an existing DrawingView object. | 
|  AddByDetailEnvelope | Creates an detail DrawingView object and a DetailEnvelope object from an existing DrawingView object. | 
|  AddByDraftView | Adds a draft view that references the same user graphics as the input draft view. | 
|  AddByFold | Creates a folded DrawingView object from an existing DrawingView object. | 
|  AddDetailView | Creates an detail DrawingView object and a DetailEnvelope object from an existing DrawingView object. | 
|  AddDraftView | Adds a scalable draft view to contain only user graphics. | 
|  AddEmptyView | Adds an new empty, out-of-date drawing view.  Specify parameters using view properties and then call Update. | 
|  AddPartView | Adds a part drawing view based on the ViewType. | 
|  AddPMIModelView | Adds an drawing view based on the specified PMI model view. | 
|  AddSheetMetalView | Adds a sheet metal drawing view based on the ViewType. | 
|  AddWeldmentView | Adds a weldment drawing view based on the ViewType. | 
|  Align | Aligns selected principal and/or auxiliary DrawingView objects that are contained in a selection set. | 
|  Item | The items in a collection. | 
|  Unalign | Removes the alignment relationship between selected principal and/or auxiliary DrawingView objects that are contained in a selection set. |