|  Application | Returns the active application object. | 
|  AssemblyFamilyMemberName | Returns the AssemblyFamilyMember name for the referenced object. | 
|  AttributeSets | Returns the AttributeSets collection object for the referenced object. | 
|  FileName | Sets and returns the file name for the referenced object. | 
|  GeometricVersion | Returns a value that is incremented each time the geometry of an associated document is changed. | 
|  IndexReference | Returns the 1 based index of the model link. | 
|  IsAssemblyFamilyMember | Returns True if the ModelLink is one of an AssemblyFamilyMember. | 
|  IsAttributeSetPresent | Returns True if a specified Attribute Set exists on the referenced object. | 
|  ModelDocument | Returns the document object of the source model file for the referenced ModelLink object. | 
|  ModelNodes | Returns the ModelNodes collection object for the referenced ModelLink or ModelNode object. | 
|  ModelOutOfDate | Returns wether or not the underlying model is out-of-date. | 
|  ModelType | Returns the model type for the referenced ModelLink or ModelNode object. | 
|  Parent | Returns the parent object for the referenced object. |