Solid Edge Draft Type Library
AttributeSets Property
Description
Returns the AttributeSets collection object for the referenced object.
Property type
Read-only property
Syntax
Visual Basic
Public Property AttributeSets As Object
Example
Private Sub Form_Load()
    Dim objApp As SolidEdgeFrameWork.Application
    Dim objDoc As SolidEdgeDraft.DraftDocument
    Dim objSheet As SolidEdgeDraft.Sheet
    Dim objModelLink As SolidEdgeDraft.ModelLink
    Dim objAttribSets As Object
    ' Local variables to be declared here
    Const TESTFILE = "T:\vbtests\testcases\chead.par"
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
        Set objDoc = objApp.Documents.Add("SolidEdge.DraftDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    On Error GoTo 0
    'Get the Active Sheet object
    Set objSheet = objDoc.ActiveSheet
    'Add a model to the Document
    Set objModelLink = objDoc.ModelLinks.Add(Filename:=TESTFILE)
    ' Get the AttributeSets property
    Set objAttribSets = objModelLink.AttributeSets
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objSheet = Nothing
    Set objAttribSets = Nothing
End Sub
See Also

ModelLink Object  | ModelLink Members

Send comments on this topic.