AdditionalSheetsBackgroundName | Gets or sets the name of background sheet for additional pages. |
AnchorPoint | Specifies which corner of the Table is the origin. |
Application | Returns the active application object. |
Cell | This read-write property specifies which cell value in the generic Table object to set or get. |
ColumnHeaderPosition | This read-write property specifies the position of the column title in the generic Table object. |
Columns | This read-only property specifies the number of columns in the generic Table object. |
CreateNewSheetsForTable | Gets or sets the option to create new sheets for each page. |
DataFixedRowHeight | Gets or sets fixed row height for data rows. |
EnableGroups | Gets or sets teh option to enable groups. |
FillEndOfTableWithBlankRows | Gets or sets the option to fill end of page with blank rows. |
FirstSheetBackgroundName | Gets or sets the name of background sheet for first page. |
GroupByColumn | Gets or sets the column to group by. |
Groups | Gets the groups collection. |
HeaderFixedRowHeight | Gets or sets fixed row height for column header rows. |
MaintainSheetsWithTableSize | Gets or sets the option to delete sheet when page is removed. |
Margin | Sets and returns the minimum distance from the extents of the OLE object to the extents of the frame boundary. |
MaximumHeightAdditionalPages | Gets or sets the maximum height of additional pages. |
MaximumHeightFirstPage | Gets or sets the maximum height of first page. |
MaximumRowsAdditionalPages | Gets or sets the maximum rows on additinal pages. |
MaximumRowsFirstPage | Gets or sets the maximum rows on first page. |
NumberOfHeaderRows | Gets or sets the number of header rows. |
PageGap | This read-write Double property specifies the spacing between multiple pages in a generic Table. |
Pages | Gets the pages collection. |
Parent | Returns the parent object for the referenced object. |
ReverseDisplayOrder | This read-write Boolean property specifies whether or not the table data is displayed in reverse order. If set to 1 (True), data in the table cells are displayed in the reverse order of entry ; if 0 (False), the are not displayed in reverse order. |
Rows | This read-only property specifies the number of rows in the generic Table object. |
ShowColumnHeader | This read-write Boolean property controls the display of column headers for the generic Table object. If this property is True, the column header is displayed; if False, the column header is hidden. |
ShowSheetBackground | Gets or sets the option to show the background sheet. |
TableStyle | This read-write String property specifies the style associated with the Table object. |
TitleFixedRowHeight | Gets or sets fixed row height for title rows. |
Titles | This read-only String property collects all titles in the generic Table obect. |
WrapDataCellsToNewRow | Gets or sets the option to wrap data cells to new row. |