Solid Edge Draft Type Library
ReverseDisplayOrder Property
Description
This read-write Boolean property specifies whether or not the table data is displayed in reverse order. If set to 1 (True), data in the table cells are displayed in the reverse order of entry ; if 0 (False), the are not displayed in reverse order.
Property type
Read-write property
Syntax
Visual Basic
Public Property ReverseDisplayOrder As Boolean
Remarks
This property does not affect the table titles.
See Also

Table Object  | Table Members  | Solid Edge V19 - What's New

Send comments on this topic.