| Solid Edge FrameworkSupport Type Library : AnnotAlignmentShape Object |
BringForward | This method brings the AnnotAlignmentShape object one more level closer to the top of the display order in the drawing view. |
BringToFront | This method sends the Connector object to the front of the display order in the drawing view. |
Copy | This method copies the AnnotAlignmentShape object onto the Windows Clipboard. |
Cut | This method copies the AnnotAlignmentShape onto the Windows Clipboard, and deletes it from the drawing view. |
Delete | This method deletes the AnnotAlignmentShape object from the drawing view. |
GetGeometry | This function returns geometry of alignment shape in form of x-y coordinates of points. |
InsertVertex | This function inserts new vertex at a location on alignment shape nearest from point formed by above x-y coordinates. |
ModifyVertex | This function assigns dNexX and dNexY value to x and y coordinates of vertex at index “nIndex”. |
Range | This method returns the coordinates of the rectangular range box bounding the AnnotAlignmentShape. |
RemoveVertex | This function removes vertex at particular index. Indices are 0 based. |
Select | This method adds the AnnotAlignmentShape object to the drawing view select set, as if the interactive user had selected it with the mouse. |
SendBackward | This method brings the AnnotAlignmentShape object one more level closer to the back of the display order in the drawing view. |
SendToBack | This method sends the AnnotAlignmentShape object to the back of the display order in the drawing view. |
Application | Returns the active application object. |
ClosedAlignmentShape | This function returns true if alignment shape is closed. |
Document | Returns the document to which the referenced object belongs. |
DrawingView | This property will get and set drawing view to which alignment shape is connected. |
FirstBalloon | This property will get and set balloon from which numbering for part list balloons will start. |
Index | Returns the numeric index for the active object. |
ItemNumberDirection | This property will get and set direction of item numbers for part list balloons connected to alignment shape. |
Key | Returns a key (a string) to find the object relative to its owning parents. |
MinimumSpacing | This property will set and get minimum spacing option on alignment shape. |
MinimumSpacingValue | This property will set and get value of minimum spacing for alignment shape. |
Name | Returns the name of the referenced object. |
Parent | Returns the parent object for the referenced object. |
Type | Specifies the type of the object being referenced. |
UniformSpacing | This property will set and get uniform spacing on alignment shape. |
VertexCount | This function returns number of points of alignment shape geometry. |
ZOrder | Specifies the front-to-back order in which an object is displayed relative to other objects. |