| Class Module | Description |
| AnnotAlignmentShape | This class is for handling individual 'AnnotAlignmentShape'. |
| AnnotAlignmentShapes | |
| AnnotInitData | Stores the data required to create an annotation. Use with AddPMIAnnotations() method. This is the only way to create PMI annotations. |
| Arc2d | An Arc2d graphic object drawn on a sheet or a profile. |
| Arcs2d | A collection of Arc2d objects. |
| AreaProperties | The AreaProperties object exposes all of the computed properties for a given set of closed boundaries. |
| AreaPropertiesCollection | The AreaPropertiesCollection object represents a collection of AreaProperties objects. |
| BackDrop | Displays graphics in a Window or SheetWindow that serves as a context backdrop for working in paper space. |
| Balloon | An annotation object that consists of text contained within a closed shape. |
| Balloons | A collection of Balloon objects. |
| BoltHoleCircle | A BoltHoleCircle object represents a bolt hole circle annotation. |
| BoltHoleCircles | A BoltHoleCircles object represents a collection of BoltHoleCircles objects. |
| Boundaries2d | A collection of Boundary2d objects. |
| Boundary2d | Represents a closed 2-D region. |
| BoundaryStyle2d | Provides properties and methods that allow you to change the Fill Style or to override the display characteristics of a Boundary2d object. |
| BoundingObjects2d | Provides access to the linear geometries that drive the Boundary2d geometry. |
| BSplineCurve2d | A multi-curved object that contains poles and transition points. |
| BSplineCurves2d | A collection of BSplineCurve2d objects. |
| CenterLine | A linear element that delineates the center of a nonlinear object. |
| CenterLines | A collection of CenterLine objects. |
| CenterMark | Consists of two perpendicular linear elements that form a crosshair pattern at the center point of a curved element. |
| CenterMarks | A collection of CenterMark objects. |
| ChamferGeometry2d | Contains methods and properties for a Line2d object defined as a chamfer. |
| Circle2d | A circle graphic object drawn on a sheet or profile. |
| Circles2d | A collection of Circle2d objects. |
| CircularPattern2d | Represents an occurrence of a circular pattern in a sheet or profile. |
| CircularPatterns2d | A collection of CircularPattern2d objects. |
| ComplexString2d | A string of endpoint-coincident 2-D geometry objects. |
| ComplexStrings2d | A collection of ComplexString2d objects. |
| ComponentImage2d | |
| ComponentImages2d | |
| Connector | The Connector object is an annotation object that connects 2D elements, objects, blocks and other annotations. |
| Connectors | The Connectors object represents a collection of Connector objects. |
| CornerAnnotation | A corner annotation on a mechanical drawing. |
| CornerAnnotations | A collection of CornerAnnotation objects. |
| Curve2d | An object that passes through a series of points. |
| Curves2d | A collection of Curve2d objects. |
| DatumFrame | A datum feature on a mechanical drawing. |
| DatumFrames | A collection of DatumFrame objects. |
| DatumPoint | An object in the DatumPoints object collection. |
| DatumPoints | A collection of DatumPoint objects. |
| DatumTarget | An object in the DatumTargets object collection. |
| DatumTargets | A collection of DatumTarget objects. |
| Dimension | Stores characteristics such as size, distance, and angle. |
| Dimensions | A collection of Dimension objects. |
| DimensionStyle | Consists of a group of parameters that control the dimension format and presentation characteristics. |
| DimensionStyles | A collection of DimensionStyle objects. |
| DimInitData | Stores the data required to create a dimension. Use with AddDimension() method. This is the only way to create PMI dimensions. |
| DimStyle | A virtual object on a specific dimension. |
| DisplayData | The DisplayData object is a temporary, virtual object that contains data about a referenced dimension. |
| DrawingObjects | Contains a single drawing object or a collection of all the drawing objects on a sheet. |
| DrawingViewStyle | Consists of a group of parameters that control the format and presentation characteristics of captions and lines of drawing views and other view annotations such as, cutting plane line, view plane line and detail envelope. |
| DrawingViewStyles | A collection of DrawingViewStyle objects. |
| Ellipse2d | An Ellipse2d graphic object drawn on a sheet or a profile. |
| Ellipses2d | A collection of Ellipse2d objects. |
| EllipticalArc2d | An asymmetrical arc graphic object drawn on a sheet or a profile. |
| EllipticalArcs2d | A collection of EllipticalArc2d objects. |
| FeatureControlFrame | A graphic object used for conveying the acceptable tolerance or variation allowd on a feature or dimension. |
| FeatureControlFrameDataSet | A collection of predefined Feature Control Frame property settings. |
| FeatureControlFrameDataSets | A collection of FeatureControlFrameDataSet objects. |
| FeatureControlFrames | A collection of FeatureControlFrame objects. |
| FilletGeometry2d | Contains methods and properties for an Arc2d object defined as a fillet. |
| Frame | Contains a set of style properties that specify how a frame is drawn. |
| GeometryStyle2d | Controls geometric characteristics for 2-D geometry objects. |
| GostWeldSymbol | Specifies all unique GOST weld types necessary in the fabrication of the weldment. |
| GostWeldSymbols | A collection of GOST WeldSymbol objects. |
| Group | An object in the Groups object collection. |
| Groups | A collection of Group objects. |
| GroupStyle | Represents the editable style characteristics of the associated Group object. |
| Image2d | An Image2d object represents an occurrence of an image file in a profile. |
| Images2d | The Images2d object represents a collection of Image2d objects. |
| Leader | A linear object that associates an annotation to a point of reference. |
| Leaders | A collection of Leader objects. |
| Line2d | A Line2d graphic object drawn on a sheet or profile. |
| Lines2d | A collection of Line2d objects. |
| LineString2d | An endpoint-connected set of lines drawn as a single object. |
| LineStrings2d | A collection of LineString2d objects. |
| PMI | |
| Point2d | A Point2d graphic object drawn in a document or sheet. |
| Points2d | A collection of Point2d objects. |
| RectangularPattern2d | Represents an occurrence of a rectangular pattern in a sheet or profile. |
| RectangularPatterns2d | A collection of RectangularPattern2d objects. |
| Relation2d | Controls the graphic behavior of one or more graphic objects. |
| Relations2d | A collection of Relation2d objects. |
| Relationships2d | A collection of Relations2d collection objects. |
| SmartFrame2d | A placeholder for an OLE object. |
| SmartFrame2dDefaults | A set of default properties that are used when an OLE object is attached to a SmartFrame2d object. |
| SmartFrame2dStyle | Holds properties to be used to determine the behavior of a SmartFrame2d object. |
| SmartFrame2dStyles | A collection of SmartFrame2dStyle objects. |
| SmartFrames2d | A collection of SmartFrame2d objects. |
| SurfaceFinishSymbol | Defines surface roughness, waviness, and any necessary machining lay markings. |
| SurfaceFinishSymbolDataSet | A collection of predefined Surface Finish Symbol property settings. |
| SurfaceFinishSymbolDataSets | A collection of SurfaceFinishSymbolDataSet objects. |
| SurfaceFinishSymbols | A collection of SurfaceFinishSymbol objects. |
| TextBox | A rectangular element that contains paragraphs of text or symbols. |
| TextBoxes | A collection of TextBox objects. |
| TextEdit | A virtual object that has common methods and properties to act on the text data of the associated text. |
| VFSet | A View Filter Set object. |
| WeldSymbol | Specifies all unique weld types necessary in the fabrication of the weldment. |
| WeldSymbolDataSet | A collection of predefined Weld Symbol property settings. |
| WeldSymbolDataSets | A collection of WeldSymbolDataSet objects. |
| WeldSymbols | A collection of WeldSymbol objects. |