| Solid Edge FrameworkSupport Type Library : AnnotInitData Object |
ClearConnectElement | Clears the connect element data. |
ClearCreationData | Resets all the data in this AnnotInitData object. |
ClearPlane | Clears the annotation plane. |
ClearTerminatorElement | Clears the terminator element data. |
SetConnectElement | Sets connect element data. Object must be 2d geometry, reference, or edge or vertex (for PMI).UseVirtualEdge is used for PMI. |
SetPlane | Sets the plane in which the annotation will be created. This is used only for creating PMI annotations. (XY plane is the default plane) |
SetTerminatorElement | Sets terminator element data. Object must be 2d geometry, reference, or edge or vertex (for PMI).UseVirtualEdge is used for PMI. |
Application | Returns the active application object. |