Solid Edge FrameworkSupport Type Library
SendBackward Method
Description
This method changes the display order of visible objects by moving the referenced object so that it is in back of the first object behind it.
Syntax
Visual Basic
Public Sub SendBackward() 
Remarks
This command is useful when objects are hiding other objects that have a lower priority display but when you do not want to send the object all the way to the back of the priority list.
See Also

AreaProperties Object  | AreaProperties Members  | Solid Edge V20 - What's New

Send comments on this topic.