Private Sub Form_Load()
    Dim objApp As SolidEdgeFramework.Application
    Dim objDoc As SolidEdgeDraft.DraftDocument
    Dim objSheet As SolidEdgeDraft.Sheet
    Dim objBalloons As SolidEdgeFrameworkSupport.Balloons
    Dim lngCount As Long
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
        Set objDoc = objApp.Documents.Add("SolidEdge.DraftDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    ' getting the Active Sheet object
    Set objSheet = objDoc.ActiveSheet
    ' getting the Balloons collection object on the active sheet
    Set objBalloons = objSheet.Balloons
    ' adding a balloon on the active sheet
    Call objBalloons.Add(x1:=0.25, y1:=0.25, z1:=0)
    ' getting the count of the Balloons on the sheet
    lngCount = objBalloons.Count
    ' USER DISPLAY
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objSheet = Nothing
    Set objBalloons = Nothing
End Sub