| Solid Edge FrameworkSupport Type Library > Balloons Collection : Style Property |
| Visual Basic |
|---|
Public Property Style As DimensionStyle |
Private Sub Form_Load() Dim objApp As SolidEdgeFramework.Application Dim objDoc As SolidEdgeDraft.DraftDocument Dim objSheet As SolidEdgeDraft.Sheet Dim objBalloons As SolidEdgeFrameworkSupport.Balloons Dim objBStyle As SolidEdgeFrameworkSupport.DimensionStyle ' Report errors Const PI = 3.14159265358979 ' Create/get the application with specific settings On Error Resume Next Set objApp = GetObject(, "SolidEdge.Application") If Err Then Err.Clear Set objApp = CreateObject("SolidEdge.Application") Set objDoc = objApp.Documents.Add("SolidEdge.DraftDocument") objApp.Visible = True Else Set objDoc = objApp.ActiveDocument End If ' getting the Active Sheet object Set objSheet = objDoc.ActiveSheet ' getting the Balloons collection object on the active sheet Set objBalloons = objSheet.Balloons ' adding a balloon on the active sheet Call objBalloons.Add(x1:=0.25, y1:=0.25, z1:=0) ' setting the Style of the Balloons collection object objBalloons.Style = objDoc.DimensionStyles(1) ' getting the style of the Balloons collection object Set objBStyle = objBalloons.Style ' USER DISPLAY ' Release objects Set objApp = Nothing Set objDoc = Nothing Set objSheet = Nothing Set objBalloons = Nothing Set objBStyle = Nothing End Sub